Solution
During the preparation for the January 2024 edition of Pitti Uomo, Signify provided LUBIAM with 3D-printed Signify myCreation Accent Track rail projectors and Signify myCreation Grand Series suspension fixtures. The golden color and texture of the fixture were chosen to match the aesthetics of the stand and enhance the design of the furniture in the center of the space on which it was suspended.
Following this successful first experience, LUBIAM renewed its partnership with Signify, choosing the Signify myCreation Grand Series suspension fixture again for the June edition of the event. At the Mantova retail location, further Signify myCreation Accent Track rail projectors were selected.
As a result of the upgrade, LUBIAM expects to achieve energy savings of more than 50%. Additionally, these fixtures are made of at least 55% recycled materials and can be reused to produce new fixtures with lighting characteristics equal to or even superior to the original ones at the end of their extended life cycle.